The SEM-SAFE® nozzle installation kit can be used for the following purposes:
- simply covering the nozzle or
- installing the nozzle in the ceiling, while also ensuring nozzle coverage
Simplicity and ease of use were key parameters in developing this solution. With the help of magnets fitted to the clamp disc, the cover plate simply ‘clicks’ and covers the installation area.
By using the nozzle installation kit, the SEM-SAFE® nozzle can be installed last and the pressure testing can be done before the nozzle is finally installed in the ceiling. With this installation solution, any maintenance and inspection as well as alteration to the ceiling can be done without interfering with the high-pressure water mist nozzle and system, thereby saving time on installation and maintenance significantly.