One fire safety technology to cover all areas in a building
The SEM-SAFE® fire hose reel cabinets can be connected directly to the high-pressure water mist piping network with very small branch pipes (OD 12 mm). Thus, a dedicated separate piping network is not needed. This means less time is spent on piping work, planning and installation as well as fewer components need to be installed on-site.
The SEM-SAFE® high-pressure water mist system and the SEM-SAFE® fire hose reel cabinet with spray gun can share the same pump unit, leaving more space for other money generating activities.
One technology serves all fire safety needs in the building, making installation, maintenance and service easier to perform.