Menu

Final SEM-SAFE® shipments for DNV-Gødstrup hospital

Published 7 July 2020

Danfoss Fire Safety is the supplier of the fire safety system installed in DNV-Gødstrup, a 145,000m2 hospital complex in Gødstrup, consisting of a 127,000m2 somatic department, 13,000m2 psychiatric department and 5,000m2 research and education centre.

DNV-Gødstrup is the patient’s hospital

The building project started in 2012 and will open in the spring of 2021. The DKK 3.2 bn state-of the-art hospital will provide more than 400 patient beds. The full focus will be on providing the best possible patient care and modern research, training and education facilities.

Danfoss and Brøndum partnership

The excellent collaboration between Danfoss Fire Safety and Brøndum, one of our business partners in Denmark, resulted in us winning the project in 2017. Thus, the SEM-SAFE® high-pressure water mist system is installed in the DNV-Gødstrup hospital, with the final components currently being delivered. Brøndum has handled the design and installation of the SEM-SAFE® system.

SEM-SAFE® in short

Over 6,300 SEM-SAFE® high-pressure water mist nozzles have been installed, covering OH1 public spaces, OH1 suspended ceiling and subfloor applications and OH4 areas. The outpatient area is covered by our 12m ceiling height SEM-SAFE® nozzle (nozzle ID= CQ). We have supplied two SEM-SAFE® high-pressure water mist pump units, each with four pumps, 120kW working in a master-slave configuration and an integrated flow test system controlling 52 sections.
The system chosen for the DNV-Gødstrup project complies with Danish rules: DBI retningslinje 254. Vandtågesystemer i bygninger”.

Click here to see video of the hospital building.
To read more about Brøndum visit their homepage.

                                                                For more information about the project, please contact Sales & Business Development Manager, Oliver Bradley at oli@danfoss.com.

 

Archives

Get in touch with us
Connect with us on Linkedin

Get in touch with us

Thank you for your interest. Have a specific need? Use below form to send us a message:

Get in touch with us
Policy *